S-Parameter Measurement Setup
Before you run OFF-State (zero bias) or ON-State (bias) S-parameter characterization tests, you must do some setup and configuration.
Software Licensing
Install the E5080A ENA Executable File
Set Up the Output Directory
Click Settings in the upper left corner of the display window, then select Global Settings. Enter the complete file path for where you want to save the measured data. For example:
Debug Mode:
Check this box to cause the system to send a SCPI SYST:ERR? command after each command to identify any errors in the system measurements. Use the IO Monitor utility in the IO Libraries Suite to monitor communication between the host PC and the DPT system test instruments and to view the error messages.
Output Directory
This field displays the current directory to store the: IV and CV, Double-Pulse Test, OnState S-Parameter, or Off-State S-Parameter test data. This folder is common to all tests.
IMPORTANT: You must provide this folder and path to the PEMG software for device modeling.
Next Steps
After initial setup, there are three main steps to running the tests:
Step 1. S-Parameter Hardware Measurement Control
Step 2. Configure S-Parameter Test Settings
Step 3. Calibrate the E5080A/B ENA or Using a Keysight E5061B ENA Vector Network Analyzer
More Information
-
Output File Structure for details on the output directory format.
-
On-State and Off-State S-Parameter Offline Mode (formerly Demo Mode) to see how to run the S-parameter demonstration.